cancel
Showing results for 
Search instead for 
Did you mean: 

CAM-16GZ driver

alex_tver
Associate II

I'm using STM32N6 with stm32-mw-camera to communicate to CAM-66GY sensor. I also have CAM-16GZ sensor, but looks like this sensor is not supported (because of VD6G_BAYER_NONE when I use vd6g driver). What are my options to integrate CAM-16GZ into the same project?
Thank you

2 REPLIES 2
MOBEJ
ST Employee

Hello @alex_tver , 

Currently, only the following camera modules are officially supported by stm32-mw-camera:

  • MB1854B – IMX335 (default)
  • ST VD66GY camera module
  • ST VD55G1 camera module

Please could u provide the exact sensor name/part number and basic details for CAM-16GZ (sensor reference, manufacturer, and a datasheet or product link). With this information, we can check if the sensor is already supported in our STM32 BSP camera drivers

Br

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.