STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to enter UART bootloader on STM32G030K6T6?

I'm trying to activate the UART bootloader after receiving input (from either a button press or from parsing a command from UART interrupt). I see from the G030x programming manual that to do so, I must set bits of the FLASH_OPTR register as nBOOT1 =...

GWork by Associate
  • 3499 Views
  • 3 replies
  • 0 kudos

FreeRTOS implementation with X-Cube-BLE2

I'm trying to implement a BLE task in my FreeRTOS application with the X-Nucleo-BNRG2A1 shield. I completed the BLE application (X-Cube-BLE2 package) without FreeRTOS and it has been working fine. For implementing the FreeRTOS, I have been looking in...

I try to implement UART DMA reception in circular buffer with reception with idle in STM32F429 Discovery with MCU Package for STM32F4 in Rev 1.27.0 . IDLE event is not called when number of recived char rise DMA_TC.

What i expect is that my interrupt callback (HAL_UARTEx_RxEventCallback) will be called with those event :DMA_Half_Transfert Complete -> OKDMA_Transfert_Complete -> OKIDLE_Event -> OKAll interrupt work individually but...1) Receive buffer is emptyI s...

Ethernet issue (STM32F7BIT)

Posted on October 12, 2017 at 14:40Hello .,I am working on STM32 MCU in our custom board, In this I am facing some issues related to Ethernet interface. I manage to generate Ethernet code using STM cube MX,(Using in RMII), The code is working but no...

USBx CDC ACM Descriptor Error in STM32F4

Following the example in STMCubeMx Azure USBx CDC ACM. it seems that I'm having trouble when the PC does not recognize the USB device slave giving me this error the there is no error in the app_usbx_device.c initialization, in terms of memory allocat...

0693W00000NqYXAQA3.png 0693W00000NqYYNQA3.png 0693W00000NqYYmQAN.png
Rhyzack by Associate II
  • 2505 Views
  • 4 replies
  • 0 kudos