STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Acknowledgement Error in CAN Communication

Hello there,I am newbie in CAN communication. Although there is no problem in loopback mode, I get acknowledgment error in normal mode. For this reason, the tx message I sent continues to be sent because it was not ACKed, and after a while, all mailb...

0693W00000QOORrQAP.png 0693W00000QOOU2QAP.png
SUrte.1 by Associate II
  • 8668 Views
  • 12 replies
  • 0 kudos

Should BSP_USBPD_PWR_VBUSOff() and BSP_USBPD_PWR_VBUSOn() of the USBPD library block until the VBUS voltage is ok?

Hi,We try to implement a DRP device with the USBPD library on a STM32G071 uC.From the documentation the requirements for the following functions are not clear:BSP_USBPD_PWR_VBUSOff():- Should it block until VBUS < USBPD_PWR_LOW_VBUS_THRESHOLD?- What ...

0693W00000Nsi0oQAB.png

How to configure USB config files to send PCM data ?

Hello everyone,I'm not new with STM32 ecosystem but this is the first time I use USB Audio Device on my MCU. I have mems mic and achieve to convert PDM to PCM data. Actually I'm trying to send them trought USB. But I can't understand what I need to e...

Axoul by Associate
  • 998 Views
  • 1 replies
  • 0 kudos

X-CUBE-CLD-GEN generic MQTT UART ISSUE

Hello I'd like to report a bug concerning the GENERIC MQTT Project.In this project one must use a serial terminal to configure wifi point by giving ssid, connexion mode ( WEP, WPA,or WPA2)and a password.The bug is that the password typing sequence is...

NBreard by Associate
  • 1443 Views
  • 2 replies
  • 0 kudos