STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32 H723ZG ethernet UDP server example

hi its been months since i started my journey with the ethernet port i need to communicate via UDP to a pc to get data from the board and send i succeeded some times where some of my projects worked for a while then stopped sometimes the board doesnt...

bakhti by Associate II
  • 6020 Views
  • 1 replies
  • 1 kudos

X-CUBE-STL - Safe Limited Speed

Hi,I would like to use the X-CUBE-STL on a STM32F446RE to trigger a STO (safe torque off) and a SLS (safe limited speed) with PLc. The STO is no problem at all, since the controller can trigger that directly by using two input GPIOs and one output GP...

HL?�t by Associate II
  • 1107 Views
  • 0 replies
  • 0 kudos

Resolved! [Solved] STM32F446 SDIO FindSCR Fifo is zero

I have a strange issue. I used the SDIO Interface on a F2 and a F429 without issues. But on the first usage with the F446 i run into a strange problem.With the Logic Analyzer i am observing the communication.Card Init:Requesting Card Type, CSD and CI...

0693W00000UoZrZQAV.png 0693W00000UoZrUQAV.png

I cannot put STM32-U575 in low power mode.

Hello,I'm testing with a NUCLEO-U575ZI-Q, I'm testing with the examples STM3Cube_FW_U5_V1.1.0.0jects_NUCLEO-U575ZI-Q. The minimum consumption I have achieved by modifying the code somewhat is 118uA seems very high to me.With other models of NUCLEO I ...

DLópe.1 by Associate
  • 1214 Views
  • 2 replies
  • 0 kudos