User Activity

 Hi all,I am taking my first steps with the STM32MP257F-EV1, following the "Let's Start" guide on the wiki.At startup, I get a blinking RED LD1, which stops blinking as soon as I connect the CN15/USB_OTG port of the STM32MP257F-EV1 motherboard using ...
Hi all,I would like to ask if there is a suggested procedure to move the network weights, the one generated inside network_data.h, to external memory-mapped QSPI FLASH. I've already moved both input/output data and activation to external SRAM, but I'...
Hello, everyone. I had a problem with version 7.1.0 of X-CUBE-AI. When I load the TFlite model of the neural network and generate the code I have problems initializing the input and output buffers. In particular I have a problem with this assignment:...
Dear all,I've been trying to generate "LL_ADC_REG_TRIG_EXT_HRTIM_TRG1" with HRTIM to trigger a dual simultaneous conversion of the ADC of my STM32G474 based project.I use LL drivers so, to my understanding the code to enable the trigger on the HRTIM ...
Hi all,after developing the firmware for a composite USB application (AUDIO + CDC_VCOM) for an STM32F446 device, I'm facing strange behaviour in the driver side for Windows (I've tested both 10 and 8 with the same results) - Linux and MacOs works out...
Kudos from