STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Reading data sent from USB_OTG_FS via PuTTY

Hi. I hope this is the right place for such a question about USB communication, I am still new to STM32.I have been trying to send a message from my STM32 board (STM32756-EVAL) without using UART, but the OTG USB. I have been trying to set up my PuTT...

OIp.1 by Associate III
  • 4072 Views
  • 5 replies
  • 0 kudos

Resolved! Bug STM32F429ZI LWIP not work after link up/down

STM32Cube FW_F4 V1.27.1HAL ETH LWIPfileethernetif.c HAL_ETH_Start(&heth); line 880 if(linkchanged)  {   /* Get MAC Config MAC */   HAL_ETH_GetMACConfig(&heth, &MACConf);   MACConf.DuplexMode = duplex;   MACConf.Speed = speed;   HAL_ETH_SetMACConfig(&...

vekli by Associate II
  • 1239 Views
  • 1 replies
  • 0 kudos

STM32F4 Ethernet issue with Cube FW_F4 V1.27.1

Hi ST guys,There seems to be an issue with the "ethernet_link_thread" generated for my particular use-case from CubeMX. As generated,the Ethernet link will not restore the link UP state after being disconnected during run time. My .ioc and workaround...

TTsek.2 by Associate
  • 4316 Views
  • 3 replies
  • 0 kudos

STM32L151c8t6: Stopping and Starting ADC with DMA with HAL functions screws up channel order when using tickless Idle of FreeRtos.

I use ADC with DMA in cirular scan mode to convert two audio-channels triggered by a timer. This all works well with expected results and quality most of the time.For power-saving reasons I have to change the clock tree in runtime. This may screw up ...

stst9180 by Associate III
  • 6692 Views
  • 6 replies
  • 1 kudos

ThreadX on STM32: RAM nearly filled up

I'm currently starting to use ThreadX / AzureRTOS on a STM32 Nucleo-H723ZG (STM32H723ZG MCU).I noticed that when loading the Nx_TCP_Echo_Server / Nx_TCP_Echo_Client projects from CubeMX, the RAM gets filled up pretty much to the top, which makes me w...

Ingenieer by Associate II
  • 3058 Views
  • 1 replies
  • 0 kudos

HAL_UART_Transmit() and HAL_UART_Receive() API

I am using Nucleo board and Tera term for serial monitorI want to do simple addition programI want to take two values from serial monitor by typing (number + Enter ) and print back its additionExpect output on Serial monitor:enter value A : 5enter v...

RS009 by Associate III
  • 1382 Views
  • 1 replies
  • 0 kudos

Resolved! How To Run 2 UCPD ports on CMSIS V1

Hey allI am building an application using a STM32G071RB with a DRP1M1 as ucpd 0 and a USBDP1 (old SNK1M1) as ucpd 1 and new to the STM UCPD worldIn an attempt to start from a working base, I used the DRP1M1_DRP example project as a starting point. Th...

IOTkid by Associate II
  • 2784 Views
  • 3 replies
  • 0 kudos