STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H747 ETH failed to ping

I used the program here https://github.com/stm32-hotspot/STM32H7-LwIP-Examples.However, after I downloaded the program to the STM32H747-Disco development board, the network could not ping through and the target host could not be accessed.May I ask wh...

YZhen.4 by Associate II
  • 1269 Views
  • 1 replies
  • 0 kudos

How many maximum usb vcom port we can create? Actually i created two vcom port with stm32l452 but not able to create third one. please suggest some help . for vcom port 3 descriptor detail given below.

/////////////////////////////////////////////////////  //Add 3 IAD class here // this one is for COM port 3  0x08, // bLength: Interface Descriptor size  0x0B, // bDescriptorType: IAD  0x04, // bFirstInterface  0x03, // bInterfaceCount  0x02, // bFun...

NMish.2 by Associate II
  • 1646 Views
  • 3 replies
  • 0 kudos

Why is the ethernet connection unstable?

I have followed the "https://controllerstech.com/stm32-ethernet-6-http-webserver-simple/" tutorial and have set up some parts on https://github.com/stm32-hotspot/STM32H7-LwIP-Examples for STM32H750B-DK and it works once on WEB SERVER not used FREERTO...

non by Associate III
  • 1068 Views
  • 1 replies
  • 0 kudos

Hello! I am getting constant ADC value through SPI when I add a debug message using UART on STM32F205 with CMSIS RTOS.

We have interfaced CS5532 using SPI which is initialized in continuous conversion mode. We read the ADC count in a task being called every 160 ms. When I add following statements in the task, the ADC count read from CS5532 becomes constant.sprintf(De...

TBhil.1 by Associate II
  • 1915 Views
  • 2 replies
  • 0 kudos