cancel
Showing results for 
Search instead for 
Did you mean: 

Hello, I am wanting to do a firmware upgrade on a STM32H7 processor through a USB connected to another microprocessor(Such as an Eval board). Are there any examples or libraries for firmware that will run on the Eval board which will upgrade the STM32H7?

RBela.1
Associate
 
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1

Not sure there is a DFU HOST, but there is a DEVICE

STM32Cube_FW_H7_V1.8.0\Projects\STM32H743I-EVAL\Applications\USB_Device\DFU_Standalone

You could perhaps have the donor device be an MSC DEVICE, and use the FW UPGRADE firm READ file/data content that way.

STM32Cube_FW_H7_V1.8.0\Projects\STM32H743I-EVAL\Applications\USB_Device\MSC_Standalone

STM32Cube_FW_H7_V1.8.0\Projects\STM32H743I-EVAL\Applications\USB_Host\FWupgrade_Standalone

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..