STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Which port number for TCP ethernet communication?

I am using an stm32h23zg, FreeRTOS plus TCP stack to create a TCP client.I checked, I can bind the socket to many values (tried 1, 52 and 1000, all 3 worked) but I couldn't find any recommendation on which port to use.On computers it is usually recom...

GGODA by Associate III
  • 2720 Views
  • 1 replies
  • 0 kudos

Resolved! Problem implementing a simple bootloader on STM32H743

Hello, I am experiencing a problem implementing a simple bootloader similar to the one showed by ST on youtube. I decided to use 32K of flash for the loader, while the remaining flash is available for the application. Linker file of the bootloader:ME...

MLang.7 by Associate III
  • 2335 Views
  • 2 replies
  • 0 kudos

Resolved! HAL_Delay(1); takes 2ms

Hello I just found out that the HAL_Delay() delay actually takes 1ms longer than the desired value. Why?STM CUBE IDE 1.9.0STM32F072RBT6

_legacyfs_online_stmicro_images_0693W00000dDT36QAG.png _legacyfs_online_stmicro_images_0693W00000dDT31QAG.png
PNova.2 by Associate II
  • 10325 Views
  • 7 replies
  • 0 kudos

USB Host mode in STM32F429ZI nucleo board

Hi I'm using STM32F429ZI Nucleo board to work on integrating C270 Logitech camera through USB host. I'm not getting any interrupt in the USB IRQ handler when the device is connected. And it is said that LD8 LED will be ON when the USB is in device or...

_legacyfs_online_stmicro_images_0693W00000dDbZZQA0.png
RAnan.3 by Associate III
  • 1818 Views
  • 2 replies
  • 0 kudos

Crash when using bootloader to turn off protection

Can anyone confirm whether my understanding of the following behaviour is correct (and whether there's any way round it):When the built in bootloader has been entered by jumping to it from firmware (i.e. the BOOT0 pin is NOT pulled high), and the boo...

s_ by Associate III
  • 1549 Views
  • 2 replies
  • 0 kudos