STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32U575i-EV Ux_Host_MSC example hard fault

Hi All,Cube MX version - 6.9.0Software Package version - 1.3.0I am using STM32U575i-EV evolution board and trying to run the Ux_Host_MSC example code.I generated the code using STM32 Cube Mx using example selector option, I generated the code for IAR...

RRajb2_0-1689681219342.png
RRajb.2 by Associate III
  • 2124 Views
  • 3 replies
  • 0 kudos

Add an Essential feature

Hello, Please add an empty function on HAL for other MCU's what doesn't have that functions.For example HAL_ICHACHE_Enable() for F1 series. This feature can help to easy porting to other series of MCUs.Thanks.

nimaltd by Senior
  • 1395 Views
  • 1 replies
  • 0 kudos

ADC-DMA Measurement and UART does not work

Hello,I want to transfer my ADC Data, which is transfered with DMA, over UART to a host.  /* USER CODE BEGIN Header */ /** ****************************************************************************** * @file : main.c * @brief ...

Patsch36 by Associate II
  • 3430 Views
  • 5 replies
  • 0 kudos

Resolved! LWIP with CMSISv1 and static memory allocation

Hello there.In my project, I am using LWIP with FreeRTOS at CMSISv1 and static memory allocation (configSUPPORT_STATIC_ALLOCATION = 1, configSUPPORT_DYNAMIC_ALLOCATION = 0). Is this a supported configuration? When I generate code, LWIP/Target/etherne...

djm by Associate
  • 3369 Views
  • 3 replies
  • 1 kudos

USB PD: Vendor_Defined_Extended Message

Hi Community!We're working with an STM32G0B1xx MCU and using USB PD v5.0.0 library from github (https://github.com/STMicroelectronics/stm32-mw-usbpd-core).I see here that USBPD_EXT_VDM = 0x1E is defined properly. However, when I use this with USBPD_D...

DDesr1_0-1690487916211.png
DDesr.1 by Associate II
  • 2171 Views
  • 2 replies
  • 0 kudos