User Activity

In the following HAL function, RTC ISR register is cleared by "Read/Modify/Write" instruction.Couldn't this cause eventual clearing of the ISR flags which may be raised by RTC periphery between "load" AND "store" ?If somebody can confirm that such si...
In the STM32L071 reference manual, there is following statement regarding STOP mode entry with HSE as a system clock:"If the application needs to disable the external clock before entering Stop mode, the HSEON bit must be first disabled and the syste...