STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! CAN protocol in normal mode on STM32F446RE

Hello ST community,I am using Nucleo STM32F446RE Board wanted to learn CAN protocol in Normal mode but i did not get any working code can you please help me to get the example code of CAN in normal mode. Thanks a lot.

Komal by Associate III
  • 1229 Views
  • 1 replies
  • 0 kudos

Hi! I found strange USB desc in SDK.

After start device, windows report about error in desc:========================== Summary =========================Vendor ID : 0x0483 (STMicroelectronics)Product ID : 0xA210USB Version : 2.00 -> wrong, Device is Full-Speed onlyPort maximum Speed : Hi...

EMaxi.1 by Associate
  • 2698 Views
  • 2 replies
  • 1 kudos

Resolved! Multiple GPIO same I2C peripheral/alternate function

Hi,Probably a dump question but wanted to make sure I got it right.On a STM32 MCU, lets sayPB0/PB1 (scl/sda) have AF4 as I2C1PB5/PB6 (scl/sda) have AF4 as I2C1If I configure all PB0/PB1/PB5/PB6 to use AF4 as I2C1,Enabling/reading/writing on I2C1 work...

LeeK by Associate II
  • 3417 Views
  • 3 replies
  • 2 kudos

STM32H743XI ADC1 ADC3 DMA data corrupted

HelloI am using  STM32H743XIH6 for Digital Power control. System clock 400MHz. ADC work clock is 36Mhz from pll2 divison. I use a external 36KHz square wave with 50% duty cycle input to GPIO_G11 to trig ADC1 and ADC3 simultaneously to converse regula...

XuanXuan by Associate
  • 835 Views
  • 0 replies
  • 0 kudos

AN5142

Where can I find example source code for AN5142 ? I try to find it in STM32Cube_FW_G4_V1.1.0 without success.

PAmsz.1 by Associate
  • 5240 Views
  • 6 replies
  • 0 kudos

Resolved! stm32f429-disc1

Can someone please tell me how to start multiple channels of  ADC? from zero using DMA? I am able to do it using the Polling method but I'm finding it difficult using the DMA

harry123 by Senior II
  • 1327 Views
  • 2 replies
  • 2 kudos

SAI witH CODEC SGTL5000

Hello,I would like to know how to recover acquisition data ​​and save the data to an SD card. I have this configurationI can compile and communicate with I2C to configure the SGTL5000 CODEC, I enabled DMA too. No errors for this moments.Thank you for...

DYann1_0-1698393813776.png
DYann.1 by Senior II
  • 1904 Views
  • 1 replies
  • 0 kudos