STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

firmware over Ethernet possible on STM32F103?

STM32F103 and W5300 (Ethernet chip) were connected to FSMC.I've officially checked how to do firmware using Uart or USB.However, I can't find the firmware method using Ethernet.Can STM32F103 proceed with firmware upgrade using firmware data received ...

DJlee by Associate II
  • 3142 Views
  • 3 replies
  • 0 kudos

Resolved! Need Help with RX ETH using HAL

Hi!!!Need assist. 2 boards with stm32F439 (Nucleo boards) direct connect1 board send packet (every 1 sec) using function:HAL_ETH_Transmit(&heth, &txConfig, HAL_MAX_DELAY);ok. packed succes captured and verified with WireShark, no errors.Try receive t...

User25 by Associate
  • 1835 Views
  • 1 replies
  • 0 kudos

STM32F103 & Encoder Mode

Dear community,I work on a 'robot' with odometrie.Each geared DC motor have a rotarty magnetic encoder ( AS5047P).I use Quadrature Output to Encoder mode. It's works but i have some questions...> get_valueWhathever the configuration on STMCube, the v...

jlecl.1 by Associate III
  • 1548 Views
  • 1 replies
  • 0 kudos

Resolved! SPI_Receive to USB_Transmit via DMA on STM32H7

Dear all,I try to read out ADC-Data, that is streamed from an external adc (AD7768) out to the uC. What I want to do is to more or less directly stream out the data via USB CDC.Therefore, I planned to use the DMA between the SPI and USB. However, thi...

Bench by Associate III
  • 7181 Views
  • 3 replies
  • 0 kudos