2022-06-26 10:11 AM
STM32CubeMX v6.5.0
STM32Cube FW_F4 V1.27.0
USB_FS HOST CDC
usbh_cdc.h
function static void CDC_ProcessReception(USBH_HandleTypeDef *phost)
line 767
if (((CDC_Handle->RxDataLength - length) > 0U) && (length > CDC_Handle->DataItf.InEpSize))
fix:
if (((CDC_Handle->RxDataLength - length) > 0U) && (CDC_Handle->RxDataLength > CDC_Handle->DataItf.InEpSize))
2022-06-26 1:18 PM
This is this line:
Can you explain a bit more, please, why there is a bug?
2022-06-26 1:38 PM
Yes. You are right line 754.
Error because length = USBH_LL_GetLastXferSize(phost, CDC_Handle->DataItf.InPipe);
and then we compare length > CDC_Handle->DataItf.InEpSize It never happens because max length is InEpSize, readings stops after first read, if you run USBH_CDC_Receive with buffer size bigger then max endpoint packet size then it will read only first packet and then reading will be stopped..
I guess that comparison needed for analyze how many bytes left for read CDC_Handle->RxDataLength
Becasue USB wok on packet basis we will continue reading if number of left bytes bigger then maximum packet size in other case we should stop reading.
2022-06-26 3:06 PM
Ah, I see. length is the last received size, and it cannot be > endpoint size.
But it can be less than the EP size, this means a short packet or ZLP, which ends the transfer.
So probably should be:
if (((CDC_Handle->RxDataLength - length) > 0U) && (length == CDC_Handle->DataItf.InEpSize))
{
//continue receiving
}
else
{
// end transfer
}@Hana Slimi what do you think?
2022-06-26 10:48 PM
I just shared my experience. In my project bug fixed with if (((CDC_Handle->RxDataLength - length) > 0U) && (CDC_Handle->RxDataLength > CDC_Handle->DataItf.InEpSize))
If you will use length == CDC_Handle->DataItf.InEpSize then you will continue reading even if requested length == InEpSize but reading should be stopped it that case.
2022-10-21 7:57 AM - edited 2025-12-10 5:29 AM
Hello @vekli,
I reported this issue internally.
Thank you for your contribution.
Internal ticket number: 137249 (This is an internal tracking number and is not accessible or usable by customers).
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-12-10 5:31 AM - edited 2025-12-10 5:31 AM
Hello;
The fix is:
if (((CDC_Handle->RxDataLength - length) > 0U) && (length == CDC_Handle->DataItf.InEpSize))
This issue is fixed: stm32-mw-usb-host/Class/CDC/Src/usbh_cdc.c at master · STMicroelectronics/stm32-mw-usb-host · GitHub
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.