STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F769I DSI SingleBuffer example with custom timing

Hello!I am working to use the STM32F769I + LCD_DSI_VideoMode_SingleBuffer code example with a different timing output. I was able to get both the 720x480 and 720x576 resolution examples working with no issue. I added a 720p resolution and also got th...

TB7 by Associate
  • 1490 Views
  • 1 replies
  • 0 kudos

Resolved! STM32H753ZI adc oversample CUBEmx error

Hello all,I bought two NUCLEO-H753ZI to experiment the ADC.Used the CUBEMX inside the STM32CubeIDE to configure the ADC to do 4x oversample (ADC1 Oversampling Ratio = "Oversampling ratio 4x").Then generated the code, but it does not compile: ... hadc...

linuxfan by Associate II
  • 1401 Views
  • 1 replies
  • 0 kudos

erase and write internal flash

Do I need to disable global interrupts for internal flash erase and write operations?  __disable_irq(); erase(); __enable_irq(); __disable_irq(); write(); __enable_irq();      

Resolved! STM32F4 EtherNet/IP library

I'm looking to use an STM32F407I for EtherNet/IP communication with some industrial motors and sensors.I cannot seem to find a library that would help me do that for the STM32F4.I found this, but I didn't really understand how to use the solution tha...

unkn0wn by Associate II
  • 5788 Views
  • 6 replies
  • 2 kudos

Resolved! LSM303DLHC STM32F411E

Hello everyone,  I am working with the STM32F411E and i am trying to make the LSM303DLHC working on my board. At this moment i am using this lib: https://github.com/STMicroelectronics/STM32CubeL4/blob/master/Drivers/BSP/Components/lsm303dlhc/lsm303dl...

ThienNguyen0301_1-1712166978775.png

What's the default value of NandFlash after erase?

Hi all,I want to access a NandFlash(H27U1G8F2B) chip which is extended by STM32F429BI's FMC;According the datasheet, seems the default value after erase is '1' for each bit.But I read the value by program is '0':My test code as below:#define TEST_NUM...

Junde_1-1716358491520.png Junde_0-1716357218449.png
Junde by Senior III
  • 1722 Views
  • 2 replies
  • 0 kudos

B-L4S5I-IOT01A

Hi,I going to choose "B-L4S5I-IOT01A" this board for my project (it is combination of ADC and IOT), can please in which IDE version having all these libraries for ADC and Wi-Fi on this board.Thanks,