STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

USBX MSC SD card + FILEX SD card problem

Hi, i'm trying to make a firmware that can read an SD card with filex but that can also connect that SD card to USBX MSC device (no simultaney). i'm able to do the two functionality in two separate firmware, but the problem is to merge. for now is su...

ABasi.2 by Senior
  • 1050 Views
  • 9 replies
  • 0 kudos

Resolved! GPIO output not working

Hi, I’m working on an STM32G491 MCU and facing an issue with GPIO PB9.In my project, I initialize PB9 as a digital output and try to set it HIGH, but the pin always stays LOW on the board.However, if I configure PB9 as input and toggle the pin extern...

STM32H5 UART DMA Error Recovery

Hello, I am working on a project using DMA and UART HD to communicate between multiple MCUs.  I have an issue where when one MCU starts up, it momentarily interrupts the UART HD bus and sometimes causes a UART and/or DMA error.Since I am using the ST...

DPade.1 by Associate III
  • 2365 Views
  • 5 replies
  • 0 kudos