STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H723 USB Example

I was trying to use the usb cdc acm example from STM32CubeMx for a Nucleo-H723ZG board. When i run the example, the device doesn't get detected at by my computer. 

jasd33p by Associate II
  • 3852 Views
  • 7 replies
  • 0 kudos

How to Reset an UART after an error

Hi,Recently, we desighed a test board with STM32F103RB for UART communication with a wireless chip, and we found that the HAL_UART_ErrorCallback is triggered occasionally (the periods of errors vary betweent tens of minutes to hundreds of minutes), t...

Chao by Senior II
  • 6212 Views
  • 4 replies
  • 3 kudos

Resolved! CMSIS DSP Library performance

I'm using the STM32F769DI and the SMT32cCube for a project which will be using the CMSIS DSP libraries in a computationally demanding application.My C code is set for fast optimisation. __FPU_USED and FPU_PRESENT are set. ARM_MATH_CM7 is defined. I c...

IWhit.2 by Associate II
  • 7389 Views
  • 7 replies
  • 2 kudos

Issue with system memory bootloader

Hello everyone!!!By using STM32F401CCU6 controller boot pind and trying to flash my program through UART, for that i have made the Boot_pin0 to high and Boot_pin1 to low and reset the controller later trying to connect with STCube programmer via UART...

Screenshot (35).png
Anil3 by Associate III
  • 2916 Views
  • 6 replies
  • 1 kudos