STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F427VGTx HAL_I2C_Mem_Write_DMA error

Hi, I have an issue using the HAL in question. I'm trying to write the following 4 characters 'C', 'i', 'a', 'o' to the EEPROM at address 0x0000, but what I observe through the analyzer is that the first character 'C' is being lost.Instead, the read ...

2024-09-13 12_41_11-Logic 2 [Logic - Connected] [Session 0].png

Resolved! Using HAL NAND

Good afternoon. I am configuring a NAND memory using FMC on the STM32H7. I am dealing with the following scenario: HCLK = 80 MHz (to match the example in AN4761) and a NAND memory SkyHigh Memory S34ML01G1 Following all the calculations specified in A...

Resolved! NUCLEO H755ZI-Q no signal on CAN TX line

Hello,I'm developing an application based on the above mentioned NUCLEO board and need a CAN connection to control the board. I've done some embedded development, but this is my first time using an STM board, so please forgive my lack of experience.I...

NUCLEO G491RE FOR PWM INVERTER

Hello,I want to generate 6 PWM signals for a 3-phase inverter, with 2 complementary PWM signals per leg, including dead-time. Is there an example or a starting point for this using the NUCLEO-G491RE?Thanks for any help.

BOOT0 pin problem on STM32F302RE

Hello, I use STM32 for years, and on a new board I use for the first time a F3 series : STM32F302REI use exactly the same schematic as all my previous board, and for the BOOT0 pin, I have a 2.2K pull-up pull-down, and a jumper to set the pin to 3.3V ...

USB_PD HPD VDM Send Attention Message

I'm working with USB_PD through a nucleo sink and a G474ER and want am receiving the ACK/Good CRC messages that are started from the laptop side (DIscover identit, discover SVID, Discover Mod, Enter Mode, dp status, dp config), but am unable to get t...

FP-AUD-AEC1 on NUCLEO-F446RE, X-NUCLEO-CCA01M1 and  X-NUCLEO-CCA02M2 following UM2824 - Rev 2 & Quick Start Guide Version 1.0 (Jan, 2021)

Hardware:NUCLEO-F446RE,  X-NUCLEO-CCA01M1,  X-NUCLEO-CCA02M2Software:Downloaded from STM: V1.2.0 and V1.1.0Github: V1.2.0 Hi, I am attempting to get sound output from the sound terminal expansion board CCA01M1 with no luck. I managed to follow UM1979...

OceanPlumber_1-1725432897717.png OceanPlumber_0-1725432879596.png OceanPlumber_2-1725433013402.png OceanPlumber_3-1725433045624.png

Resolved! STM32U535CET6 USBX

Hello,I'm trying to get USBX CDC Virtual COM Device configured on an STM32U535CET6.  I have downloaded and tried to play matchup with the projects out on GitHub for the U5 series but have had no success.  I'm currently stuck on: /* Now check for inva...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.