STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Looking for PVD example with STM32G0

hello!  i have a question about the power voltage detector in (external input analog voltage) i have a adjustable power supply connected on the pin (using a nucleo-G0B1RE) i was thinking that if i drop the voltage on the pin under the vref int voltag...

ABasi.2 by Senior
  • 1711 Views
  • 2 replies
  • 0 kudos

STM32L452 TouchGFX and SD Card

Hello,I am using a custom board with the STM32L452RET. On this board:SPI1 is connected to an IIS3DWB accelerometer,SPI2 is connected to a 240x280 TFT display with an ST7789 controller and TouchGFX,SPI3 is used with FatFs to access an SD card, followi...

fmaesso by Associate II
  • 1811 Views
  • 1 replies
  • 0 kudos

STM32F070CBT6 Emulate Eeprom Issue

When using this microcontroller for emulate eeprom process, i got some problems like freezing at start-up, when writing OLED, sprintf function can not write characters- writes silly words. I am not sure if the problem is about my emualte_eeprom proce...

Resolved! PPPos Lwip Issue

Hello everyone,Today I'm writing to you because I'm trying to implement a PPPoS connection over the USB CDC Host of a STM32H745. The modem I'm trying to connect to is a SIM7500 of SimCom.I managed to establish the connection between the modem and the...

RPC by Associate III
  • 2764 Views
  • 4 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.