STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32 G4 HAL i2c not clearing interrupts

**Problem:**- When the I2C is enabled, the part can hit the WWDG.- It looks like the pointer to the function `XferISR` is getting set to NULL somehow.  - When this happens, the interrupts are not cleared, and it continually fires the interrupt becaus...

photon by Associate
  • 2390 Views
  • 3 replies
  • 0 kudos

LWIP for F767ZI

Hi y'all, is there a IOC file or way to setup the LWIP + RTOS + NETCONN example via IOC for STM32F767ZI? I have it completely working based on the example with no IOC, but that makes this code hard to scale and move across multiple machines. I notice...

STM32F7 Ethernet on bare metal without Cubemx

Hi Team,I am Using STM32F7 nucleo board, I created project using ST CUBEIDE version 1.16.0.Note: NOT USING CUBEMX and RTOSI have taken a ref code for low level eth functions ethernetif.c and lwip.c.I Enabled Enable DHCP, Http and SSI it is working fi...

lavanya by Associate III
  • 5445 Views
  • 6 replies
  • 2 kudos

Resolved! Cannot Extract STSW-SAFEA1-MW

Hi,I am having trouble extracting the STSW-SAFEA1-MW. This is the same issue mentioned here and here. I can't use your product if I can't use your drivers. A fix would be appreciated.Thanks