STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

FATFS: f_mkfs not working.

Hi,I use STM32Cube, STM32CubeIDE and my board is STM32F746. How do I update FATFS? The system is running version 0.12c. This is from 2017.Why do I want to update it?After inserting the SD card, I check the status and if the card is not formatted, I w...

JNova.0 by Associate III
  • 3000 Views
  • 6 replies
  • 1 kudos

Resolved! USB Host USBH_HID_SetReport function issue

Hi, I am using an STM32G0B1CT6 and generated code using the STM32CubeMX to use the USB Host library to interface the CP2112 device. I am able to enumerate and communicate with the device using the interrupt IN/OUT. I am also able to get reports using...

DDeba.1 by Associate III
  • 1378 Views
  • 3 replies
  • 1 kudos

Resolved! GPIO HAL Sanity Check

I need a second pair of eyes. I am trying to setup EXTI using the GPIO HAL. But it looks like its doing it wrong. It must be me but I need you to double check to be sure.This is STM32G0 HAL so stm32g0xx_hal_gpio.c /*--------------------- EXTI Mode Co...

Carl_G by Senior III
  • 2468 Views
  • 7 replies
  • 0 kudos