STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LWIP Free RTOS Problem

Hi. I have a problem while using lwip and freertos. The board is based on stm32h743vih. The mpu configuration is done correctly i think. My problem is after i start udp server and start to send data with udp, everything is ok, but after a while i wil...

Resolved! How to make the FDCAN with DMA.

Hi, I'm not able to find any DMA available with CAN peripheral in STM32G4. After going deep search I found there's no such native DMA request available for CAN peripherals. So, I want to know is it true that STM32 controllers don't come with DMA with...

Resolved! X-CUBE-CRYPTOLIB first computed SHA256 hash wrong

Hello,I would like to use the X-CUBE-CRYPTOLIB to calculate a SHA256 with a key, i'm using STM32CubeIDE 1.18.0 for an STM32u083 microcontroller, STM32CubeExpansion_Crypto_V4.2.0.The issue I have is the first time I call cmox_mac_compute the wrong res...

POliv by Associate III
  • 2958 Views
  • 10 replies
  • 4 kudos

STM32H747 lwip - freeRTOS

Hi, I am developing firmware for an STM32H747 with Ethernet connected via RMII to a LAN8742 PHY. The project uses lwIP and FreeRTOS. UDP communication works fine when sending data, but when receiving UDP packets, the system crashes after some rundom ...

luca_sc by Associate
  • 1104 Views
  • 1 replies
  • 1 kudos

I3C LL_I3C_ControllerHandleMessage Problem

I am using the STM32H523 microcontroller with I3C function and a system clock of 250MHz. I am configuring LL-I3C_SetPeriodClockHighI3C (I3C1,0x0D) based on the LL library;LL_I3C_SetPeriodClockLowPP(I3C1,0x0D);LL_I3C_SetPeriodClockLowOD(I3C1,0x0D);At ...

CornOnly by Associate
  • 874 Views
  • 1 replies
  • 0 kudos