STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Calculate MD5 Hash in chunk

Hello, I'm trying to use the HAL function to calculate a file MD5 on my STM32H750 MCU. I successully managed to calculate the MD5 of little files using HAL_HASH_MD5_Start. Now I want to calculate the MD5 of a large file, so I'm not able to store all ...

STM32H7 MIPI DSI maximum clock speed?

There is inconsistency in the reference manual and the STM32CubeMX clock configuration tool as to what the maximum clock for the PLL DSI. Reference manual suggests it is 1000 MHz however, when set to that in STM32CubeMX, an error is generated at the...

bchia by Associate
  • 6267 Views
  • 10 replies
  • 1 kudos

STM32H745ZITx - USART RX DMA Not Working

Hello,I'm working with the STM32H745ZITx and trying to receive data over USART3 using RX DMA. However, the usart_rx_dma_buffer remains all zeros — as if no data is written. Here’s what I’ve checked::small_blue_diamond: DMA Configuration:DMA1_Stream0,...

Input Capture - Trouble Measuring Frequency

Hello, i have been trying to measure the frequency of a pwm signal using input capture. I am using Nucleo-F429ZI I want to print the values of the frequency of the signal in question with UART. The frequency of my signal is 100 kHz but I read stuff l...

toti by Associate
  • 670 Views
  • 3 replies
  • 1 kudos

Ethernet problem on STM32H747I-DISCO board

Hi everyone,I have a problem with the Ethernet connection that I can't solve on the STM32H747I-DISCO board.I followed Adam Berlinger's guide step by step (https://community.st.com/t5/stm32-mcus/how-to-create-a-project-for-stm32h7-with-ethernet-and-lw...

magianf by Associate II
  • 1713 Views
  • 7 replies
  • 1 kudos