2025-08-04 9:11 AM
I'm working on building an Ethernet infrastructure using LWIP on an STM32H7 series MCU for various purposes. In this setup, I want to avoid using malloc, and instead rely entirely on LWIP’s memory pool system for all memory allocations. Here's the configuration I’m planning to use:
MEM_LIBC_MALLOC 0 // Don't use the standard malloc (i.e., disable mem_malloc from libc)
MEMP_MEM_MALLOC 1 // Use mem_malloc for allocating MEMP pools
MEM_USE_POOLS 1 // Redirect mem_malloc calls to the defined memory pools
MEMP_USE_CUSTOM_POOLS 1 // Enable support for user-defined custom pools
MEM_USE_POOLS_TRY_BIGGER_POOL 1 // Allow searching for a larger pool if neededIn lwippools.h, I’ll define custom pools with different sizes like this:
LWIP_MALLOC_MEMPOOL_START
LWIP_MALLOC_MEMPOOL(24, 128)
LWIP_MALLOC_MEMPOOL(16, 256)
LWIP_MALLOC_MEMPOOL(8, 512)
LWIP_MALLOC_MEMPOOL(4, 1024)
LWIP_MALLOC_MEMPOOL(4, 1536)
LWIP_MALLOC_MEMPOOL_END
For RX, I will use the following structure from STM's LWIP examples:
#define ETH_RX_BUFFER_CNT 8U
LWIP_MEMPOOL_DECLARE(RX_POOL, ETH_RX_BUFFER_CNT, sizeof(RxBuff_t), "Zero-copy RX PBUF pool");
__DMA_RAM extern u8_t memp_memory_RX_POOL_base[];
I have three questions:
The following two options seem to contradict each other: MEMP_MEM_MALLOC = 1 and MEM_USE_POOLS = 1. Will this configuration work as I intend (i.e., using mem_malloc() but redirecting it to pools)?
If it does work, do I still need the memory space defined by PBUF_POOL_SIZE? Can I set this to 0? In other words, does my configuration allow LWIP to use only the custom pools defined in lwippools.h instead of the default PBUF_POOL memory?
In this configuration, will LWIP allocate MEMP_NUM_.. defined pool items (e.g., MEMP_NUM_TCP_PCB, MEMP_NUM_NETBUF, etc.) from the default static MEMP pools, or will those also be served from the custom pools defined in lwippools.h?
2025-08-06 5:28 AM - edited 2025-08-06 5:28 AM
Hello @SSone.1, and welcome to ST Community!
After reviewing the LwIP init.c file, the memp sanity checks show that MEMP_MEM_MALLOC and MEM_USE_POOLS cannot be used together. So, to answer your first two questions, no, it does not work that way. Regarding your third question, MEMP_NUM_* allocations come from custom pools, using the smallest pool that fits the required length.
Best regards,