STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

virtual COM port installation

Posted on February 13, 2012 at 07:19from CD00158241.pdf   ''To install the software driver of the Virtual COM port, download and execute the �Virtual Com Port Driver Setup� from the STMicroelectronics website: www.st.com. At the end of the installa...

STM32F103RB capable of USB Host?

Posted on February 14, 2012 at 22:49Title says it all. I'm looking at purchasing a USB host stack, and one of the vendors mentioned that perhaps the F103 doesn't support Host mode.  I'm just trying to do something simple:  datalogging to a USB flash...

mtanner by Associate
  • 2377 Views
  • 2 replies
  • 0 kudos

How to dump ULPI PHY registers

Posted on January 20, 2012 at 05:00I need to dump ULPI PHY registers. I use STM32F207IGT6 and STmicro provided USB library. Device is in MSC mode. I was trying to find it out myself but code is quite convoluted. Thanks. #ulpi #usb #stm32f20

dragan by Associate II
  • 571 Views
  • 0 replies
  • 0 kudos

Stack Corruption - FreeRTOS

Posted on January 02, 2012 at 05:47Hello, We are working on the STM3220-G Evaluation Board. We are using IAR compiler [V6.2] and running a test application with FreeRTOS [7.0.2] and following is the issue: 1. Used sample application code from ST lib...

girish by Associate II
  • 3539 Views
  • 6 replies
  • 0 kudos

Re-sign DFU-driver

Posted on August 24, 2011 at 12:17Hello, for my device I got the license key for my VID/PID and changed the STtub.inf, but now the DFU-driver is unsigned (because of the change). I use the same STTub30.sys-file, so I think a re-sign of the driver pa...

Pb with FreeRTOS and USB

Posted on January 05, 2012 at 13:26Hello, We are working on the STM3220-G Evaluation Board. We are using IAR compiler [V6.2] and running a test application with FreeRTOS [7.0.2] and the STM32_F105-07_F2xx_USB-Host-Device_Lib_V2.0.0 The USB is used a...

serge23 by Associate II
  • 2429 Views
  • 5 replies
  • 0 kudos