User Activity

Posted on May 13, 2013 at 07:16Hello all, I can't flash my program using ST-LINK in IAR. STM32 ST-LINK Utility can flash it, and after that I can debug my program in IAR, watch registers, put breakpoints and so on. Is it possible to flash program vi...
Posted on March 01, 2013 at 12:08I'm using drivers from VCP_V1.3.1_Setup.exe. It works fine on win7 x32, but on w8 x64 installator says something like ''it was supposed to run me under x32'', so my device does not work there. Where I can download su...
Posted on February 13, 2012 at 07:19from CD00158241.pdf   ''To install the software driver of the Virtual COM port, download and execute the �Virtual Com Port Driver Setup� from the STMicroelectronics website: www.st.com. At the end of the installa...
Posted on September 28, 2011 at 08:00some part of my code keeps the speed of motor using encoder. I have an timer interrupt, calc impulses from the motor and find the speed. It works fine in ''download and debug'' (IAR + jetlink). But when I press '...