User Activity

Posted on June 08, 2015 at 10:43HelloSTM32L0 CUBE pack, file stm32l0xx_hal_gpio.c have a mega-bug. When will be used GPIO EXTI function, at end of config the all SYSCFG->EXTICR registers will be set to FFFF.in file, function HAL_GPIO_Init:259:   tem...
Posted on May 15, 2013 at 11:24Hello! As I understand, the FOC library doesn't work right for AC induction motors, but the older library (v2.0) works well. Maybe someone in forum have in archive the older library? If it possible, please send me the...
Posted on March 13, 2012 at 16:47Hello! I have a question to STM32xx chip manufacturers. Last yar I uses STM32F10xx chips in my applications. It's 8mHz HSI works perfect - stable, with small temperature sensistivity - works very well.  CAN bus (slow...
Posted on August 12, 2011 at 19:06Hello.I have a problem with starting OTG FS in Device mode. I will try to adapt project example ''STM32_USB-FS-Device_Lib_V3.3.0'' for this STM32F-2 chip, but USB doesn't run. For new chip I'll do next: 1. Prepare s...
Posted on July 01, 2011 at 21:56Hello! I did try to use Virtual COM port project from archive STM32_USB-FS-Device_Lib_V3.3.0, loaded from site. But have problem - when MCU do sending ''bytes string'' from MCU to PC with length 0x40, 0x80, 0xC0 - PC ...