STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

USB VCP bluescreens on Windows wake-up from standby

Posted on June 27, 2014 at 13:13Hi,we are experiencing some problems with the STM32 VCP USB driver in combination with windows stand-by. When the computer wakes up from stand-by, we get a blue screen withBUGCODE_USB_DRIVER The caller has submitted a...

manuel2 by Associate
  • 764 Views
  • 0 replies
  • 0 kudos

STM32F427 HAL I2C Slave

Posted on May 13, 2014 at 09:44Hello I work with STM32CubeMX with Keil and to realize a I2C Slave withe the STM32F427. I have 2 questions: STM32CubeMX: I2Cx Configuration: Primary slave address is a 7bit value --> 0..127 In the file stm32fxx_hal_i...

How to disable USB port through software

Posted on June 25, 2014 at 12:46Sir,I have successfully initialized USB port on Hi mini STM32F1V board now I would like to design a software routine to disable the initialized USB port plz help me out how to implement this.Regards  #stm32f1-usb-p...

soobia by Associate II
  • 1062 Views
  • 1 replies
  • 0 kudos

Basic USB CDC Project

Posted on April 30, 2014 at 08:23Hi Everybody, I'm trying to get a basic USB communications device class device project working using the STM32F429I-Disco board. I'm using  smt32cube application to generate the code for the Keil uVision environment....

kabla002 by Associate
  • 3250 Views
  • 5 replies
  • 0 kudos

Ethernet Connectivity problem

Posted on June 14, 2014 at 12:19Hi Everyone,We are developing Vibration Analyzer. As a part of communication we are using Ethernet[STM32F107RCT6]. It is working fine but problem is when we unplug LAN cable from the system and plug it after 20 second...

rags by Associate II
  • 2608 Views
  • 7 replies
  • 0 kudos

Problem with running example described in the AN3966

Posted on February 05, 2014 at 12:38HelloI�m trying to run example project described in application note AN3966. According to the release note FreeRTOS project of web server using sockets contains:� Cortex-M CMSIS V3.01 � STM32F4xx CMSIS V1.1.0 � ST...

kkawula by Associate II
  • 1675 Views
  • 2 replies
  • 0 kudos

printf over USB VCP

Posted on June 19, 2014 at 13:37Hi all,I am trying to retarget printf over USB-VCP and I am stcuk !I implemented the putc function in the following way:****************************************int fputc(int ch, FILE *f){  USBD_CDC_SetTxBuffer(&hUSBDD...

HID host bug

Posted on June 01, 2014 at 18:48Hi, I have a problem that looks like a bug in STM USB library. I am using version 2.1 running on STM32F207. The problem I am facing is as follows: I have a host running at the STM32F207 (HS) and a mouse connected to i...

noam by Associate II
  • 3334 Views
  • 6 replies
  • 0 kudos