STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Making internal FLASH as MSC

Posted on September 04, 2014 at 11:02I download STM32CubeF4 from http://www.st.com/web/en/catalog/tools/PF259243. There is an example of MSC in \STM32Cube_FW_F4_V1.3.0\Projects\STM324xG_EVAL\Applications\USB_Device\MSC_Standalone\MDK-ARM.If I build ...

STM32 With Ethernet MAC & PHY

Posted on September 02, 2014 at 14:37Hi Is there a version of STM32 -cortex-M4 preferd- with Ethernet MAC and PHY. Just put the magnetic interface off chip? Regards Hossam ALzomor #ethernet-stm32

zomorh by Associate
  • 1110 Views
  • 1 replies
  • 0 kudos

STM32F4 Cube lwip Examples

Posted on September 01, 2014 at 05:29So, I've just downloaded and started playing with STM32F4 Cube's *version 1.3.0) Ethernet examples on my STM3240G-Eval. The LwIP_HTTP_Server_Raw works, but not a single one of the others does. Some debugging show...

How to flash external flash with DfuSe?

Posted on August 27, 2014 at 16:41Hi All I'm working with Keils' Eval Board MCBSTM32F200 which has external NOR Flash attatched to the STM32F207IG. For my final application I would like to use the DfuSe Mode to upgrade my firmware which is located o...

b_ by Associate II
  • 2565 Views
  • 4 replies
  • 0 kudos

STM32F4 Ethernet access after FLASH Erase

Posted on August 27, 2014 at 17:20I have a project that needs to erase FLASH sectors so that configuration data can be updated. The device is being accessed via ethernet. In the past, I was just polling the DMA status to access an incoming packet. T...

cwparker by Associate II
  • 2679 Views
  • 7 replies
  • 0 kudos

Problem using USB in Nucleo F302R8

Posted on July 19, 2014 at 23:29Hi all, I'm using the Nucleo F302R8 to build the firmware for a new board I'll develop using the same MCU. I'm trying to use USB CDC to have a VCP. I've started with CubeMX with the Nucleo F302R8 template, changed th...