STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Problem in FreeRTOS+cubef4+usb host

Posted on July 02, 2014 at 16:55I choose USB host MSC + FREERTOS+FATFS . make a project and compile it . but when i connect a USB flash , it dose not  work. but when I don't choose FreeRTOS , It worked. why ? #usb-msc-mass-storage #stm32f4-disco...

CDC Host for STM32F407

Posted on May 12, 2014 at 22:12Hi, I'm going to implement CDC Host on STM32F407 using OTG_HS. I looked for some examples, but not found any source, only advices how to modify MSC Host on STM32_USB-Host-Device_Lib_V2.1.0... Also I noticed, that there...

antony by Associate II
  • 1536 Views
  • 3 replies
  • 0 kudos

STM32 Cube USB Host wmaxpacketsize problem

Posted on August 14, 2014 at 00:13Hi, I use STM32F205ZE USB FS Host library for UVC device. Some UVC device has ISOC EP wMaxPacketSize=192Bytes, but others device's wmaxpacketsize > 500Bytes.I can get JPEG stream if device wMaxPacketSize=192Bytes or...

emre by Associate II
  • 2371 Views
  • 3 replies
  • 0 kudos

Variable-size Rx on UART using Interrupts

Posted on August 18, 2014 at 18:19I need to implement the reception of messages on UART using interrupt and the HAL set of drivers. Messages can be of varied length, but they have a terminating character. My problem is that HAL_UART_Receive_IT() tak...

dbegun by Associate II
  • 4017 Views
  • 9 replies
  • 0 kudos

STM32F207 low level ethernet driver documentation

Posted on August 18, 2014 at 05:35Hi, Does anyone know if further documentation is available for the Stm32F2x7 low level Ethernet Driver as used in the STSW-STM32060 / AN3384 LwIP TCP/IP stack demonstration for STM32F2x7xx microcontrollers.  The AN3...

martin by Associate II
  • 912 Views
  • 0 replies
  • 0 kudos

STM32F429xx/39xx Native Bootloader

Posted on August 13, 2014 at 16:18Hello guys,Ive been looking into the STM32F429xx/39xx native bootloader.To serve as a guide, here are the steps to be able to use the native bootloader:1. Jump to BTL mode, in this MCU version the best way (personal...

afduarte by Associate II
  • 2744 Views
  • 7 replies
  • 0 kudos

USB_FS SendReport data loss

Posted on August 13, 2014 at 13:32Hi,While I'm trying to send some test value through USB (using USBD_HID_SendReport -> comes from STCube library) first few data is being lost but I don't know while.Here are my descriptor:HID_DEV_ReportDesc[HID_DEV_...

licencje1 by Associate II
  • 1347 Views
  • 4 replies
  • 0 kudos

USB_FS Endpoint IN/OUT addresses

Posted on August 12, 2014 at 15:40Hi,Could somebody tell me where may I find some information about range of addresses of endpoints? In reference manual for stm32f4 I find out that there are ontly 3 in/out endpoints.In example application IN endpoin...

licencje1 by Associate II
  • 1767 Views
  • 2 replies
  • 0 kudos