cancel
Showing results for 
Search instead for 
Did you mean: 

Virtual com port driver VCP_V1.3.1_Setup_x64.exe installation

ole2
Associate
Posted on August 29, 2014 at 09:35

Hi

I am trying to install the virtual com port driver VCP_V1.3.1_Setup_x64.exe on a computer running 64-bit windows, however the installer exits after a short while with the error code:

1607: Unable to install InstallShield Scripting Runtime.

I have tried to run installer as administrator and various types of compabillity modes, but with no success. 

 

In order to investigate the problem further I have enabled windows installer debugging, this creates a log like this:

=== Verbose logging started: 29.08.2014  07:45:03  Build type: SHIP UNICODE 5.00.7601.00  Calling process: C:\Users\me\Desktop\VCP_V1.3.1_Setup_x64.exe ===

MSI (c) (9C:50) [07:45:03:825]: Resetting cached policy values

MSI (c) (9C:50) [07:45:03:825]: Machine policy value 'Debug' is 0

MSI (c) (9C:50) [07:45:03:825]: ******* RunEngine:

           ******* Product: C:\Users\me\AppData\Local\Temp\_isE80E\ISScript8.Msi

           ******* Action: 

           ******* CommandLine: **********

MSI (c) (9C:50) [07:45:03:825]: Client-side and UI is none or basic: Running entire install on the server.

MSI (c) (9C:50) [07:45:03:825]: Grabbed execution mutex.

MSI (c) (9C:50) [07:45:03:872]: Cloaking enabled.

MSI (c) (9C:50) [07:45:03:872]: Attempting to enable all disabled privileges before calling Install on Server

MSI (c) (9C:50) [07:45:03:872]: Incrementing counter to disable shutdown. Counter after increment: 0

MSI (s) (24:18) [07:45:03:872]: Running installation inside multi-package transaction C:\Users\me\AppData\Local\Temp\_isE80E\ISScript8.Msi

MSI (s) (24:18) [07:45:03:872]: Grabbed execution mutex.

MSI (s) (24:88) [07:45:03:872]: Resetting cached policy values

MSI (s) (24:88) [07:45:03:872]: Machine policy value 'Debug' is 0

MSI (s) (24:88) [07:45:03:872]: ******* RunEngine:

           ******* Product: C:\Users\me\AppData\Local\Temp\_isE80E\ISScript8.Msi

           ******* Action: 

           ******* CommandLine: **********

MSI (s) (24:88) [07:45:03:872]: Note: 1: 2203 2: C:\Users\me\AppData\Local\Temp\_isE80E\ISScript8.Msi 3: -2147286960 

MSI (s) (24:88) [07:45:03:872]: MainEngineThread is returning 1620

MSI (s) (24:18) [07:45:03:872]: User policy value 'DisableRollback' is 0

MSI (s) (24:18) [07:45:03:872]: Machine policy value 'DisableRollback' is 0

MSI (s) (24:18) [07:45:03:872]: Incrementing counter to disable shutdown. Counter after increment: 0

MSI (s) (24:18) [07:45:03:872]: Note: 1: 1402 2: HKEY_LOCAL_MACHINE\Software\Microsoft\Windows\CurrentVersion\Installer\InProgress 3: 2 

MSI (s) (24:18) [07:45:03:872]: Note: 1: 1402 2: HKEY_LOCAL_MACHINE\Software\Microsoft\Windows\CurrentVersion\Installer\InProgress 3: 2 

MSI (s) (24:18) [07:45:03:872]: Decrementing counter to disable shutdown. If counter >= 0, shutdown will be denied.  Counter after decrement: -1

MSI (s) (24:18) [07:45:03:872]: Restoring environment variables

MSI (c) (9C:50) [07:45:03:872]: Decrementing counter to disable shutdown. If counter >= 0, shutdown will be denied.  Counter after decrement: -1

MSI (c) (9C:50) [07:45:03:872]: MainEngineThread is returning 1620

=== Verbose logging stopped: 29.08.2014  07:45:03 ===

I have searched the internet and found that that the fault code returned by MainEngineThread, 1620 means: 

ERROR_INSTALL_PACKAGE_

INVALID. 

I have googled this fault code, but with no success. Does anyone have any idea what could be causing this errors?

Thanks for all help:)

#stm32 #vcp #usb
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
tsuneo
Senior
Posted on August 29, 2014 at 16:42

ERROR_INSTALL_PACKAGE_INVALID means corrupted MSI file.

Download it again from the ST’s site,

http://www.st.com/web/en/catalog/tools/PF257938

The installer on above link runs on my Win7 (x64) without any error.

Tsuneo

Posted on August 29, 2014 at 16:44

Check also if your AV software is interfering with the file(s), and put them in a real directory, not the desktop.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
ole2
Associate
Posted on September 01, 2014 at 10:30

Hi

Thank you:)

Disabling the AV software seemed to do the trick:)

Regards Ole