Posted on July 05, 2016 at 16:57Hi All I'm using the BlueNRG Chip together with the LightBlue iOS app. I was able to set up 2 services (Device Information and Battery Service). However the LightBlue app states ''No Service'' but when I connect both ...
Posted on August 27, 2014 at 16:41Hi All I'm working with Keils' Eval Board MCBSTM32F200 which has external NOR Flash attatched to the STM32F207IG. For my final application I would like to use the DfuSe Mode to upgrade my firmware which is located o...
Posted on July 28, 2014 at 11:40 Hi All,
I'm trying to use the ADC1 GPIO G8 from the STM32F207IG.
Unfortunately I don't get it working and maybe someone could help me.
The basic problem is that all ADC_*** registers getting updated e...
Posted on February 11, 2014 at 14:00
Hi all,
I'm trying to use the SPI interface on a STM32F207 with CMSIS.
Below you my sample code can be seen. The problem there is that within the function drv_Info->SendData(...) the function wait...
Posted on August 29, 2014 at 11:30Hi clive1 Thank you I got the whole project and now trying to get it running on my STM32F207. Many thanks for your help. Cheers Ben
Posted on August 28, 2014 at 07:57Hi clive1 Thank you for your quick answer. Your stated dfu-File leads to a ST user manual http://www.st.com/st-web-ui/static/active/en/resource/technical/document/user_manual/CD00196451.pdf where a screen shot shows...
Posted on April 10, 2014 at 15:39Hi I experience exactly the same problem. Calling the bootloader with the YouTube Code gives me an unenumerated USB device. Using the Boot pin work fine.