STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32 USB DFU and User application

Posted on July 21, 2011 at 11:24Hi AllI'm trying to develop a new firmware using USB DFU as well as USB MIDI class.I'm using IAR EWARM, compiling for STM32L152I downloaded the DFU project from ST libraries, and I have a couple of questions regarding...

jerome2 by Associate II
  • 611 Views
  • 0 replies
  • 1 kudos

USB HID on STM32 CL and MD

Posted on July 15, 2011 at 15:31Hello, I'm stucked at programming a USB. Based on ST USB Library and sample project (Custom HID) i've created an program that send to PC data in report of size 10 bytes. So i changed an description of usb (in usb_desc...

mpachock by Associate
  • 944 Views
  • 3 replies
  • 0 kudos

ethernet project using stm3210b-eval

Posted on June 18, 2011 at 06:55hi everybody, I have a stm3210b-eval board and I want to design a project which contains an ethernet port.I know that this board doesn't support ethernet port. could I add any external ICs to this board to have ethern...

COM over USB sending unexpected packages

Posted on June 28, 2011 at 16:48Hello everybody, I'm using STM32F103ZEH6. The device is connected to a host pc via USB emulating a virtual COM port. From time to time I can detect 2 similar packages with my USB-Sniffer an the host pc recognizes them...

stm32w IAP BOOTLOADER protocol

Posted on July 06, 2011 at 20:03Hi,Please, witch protocol uses stm32w device if nBOOT is selected (and serial-link-bootloader is selected) ? Is it USART protocol used in the STM32� bootloader (AN3155) ? Because, my stm32w device in bootloader mode r...

petr2399 by Associate II
  • 1011 Views
  • 3 replies
  • 0 kudos

Problem when trying to change USB VID for DFU

Posted on May 31, 2011 at 14:13Hello, I want to change USB VID on our device. So VID is changed in DFU_DeviceDescriptor[] in usb_desc.c. Also, I changed DFU_StringVendor[], DFU_StringProduct and DFU_StringSerial[]. StringVendor = StringProduct, Str...

jeba by Associate II
  • 1419 Views
  • 2 replies
  • 0 kudos

rewrite bootlosder

Posted on May 29, 2011 at 14:02Hi, I need to add a decryption mechanism to the bootloader firmware. 1. Is it possible to wirte a new bootloader firmware to ''system memory'' adreess 0x1FFF F000 - 0x1FFF F7FF (instead of the existing one)? 2. Can i g...

ybitton by Associate II
  • 901 Views
  • 4 replies
  • 0 kudos

flash loader demonstrator

Posted on May 19, 2011 at 15:27Hi, I am using ev board for stm32 md value line. I would like to check its bootloader option. From reading arround i saw there is a pc program named:flash loader demonstrator (by ST) where can i download it from? Thank...

ybitton by Associate II
  • 1239 Views
  • 4 replies
  • 0 kudos