STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

USART Baud rate (stm32L0 + 32kHz LSE)

Posted on February 02, 2016 at 10:34Hello, cubemx shows that baud rate for USART clocking from LSE  must be between 32 Bits/s and 131.062 KBits/s.  Is it CubeMX bug or L-series allows clocking regular USART (not LPUART) up to 130KBits?  MCU: stm32L0...

mailbox by Associate II
  • 2220 Views
  • 4 replies
  • 0 kudos

Wake from standby issues

Posted on March 20, 2016 at 20:28 Hi all, I have a few problems with waking from Standby. I use STM32L152, IAR V7.5, the MCU has constant power supplied to it. I have a custom bootloader. If my MCU has only the bootloader I d...

STM32 RTOS os_error

Posted on March 21, 2016 at 18:34 Hey there guys. Im trying to launch the OS at my brand new STM32F100 discovery (http://www.st.com/web/en/catalog/tools/FM116/SC959/SS1532/PF250863?sc=stm32-discovery) I'm handling some difficulties from be...

e239955 by Associate II
  • 1599 Views
  • 2 replies
  • 0 kudos

CUBEMX example USB CDC to UART

Posted on March 18, 2016 at 14:42Hello,i'm trying to make a USB cdc virtual port to transfer data to uart and back. I have successfully made the virtual port using CubeMX and transfer data to uart. But i have trouble to read data from uart and trans...

Bug in STM32Cube HAL

Posted on March 19, 2016 at 22:33 STM32CubeF7 v1.3.0. File:stm32f7xx_hal_i2c.c. Line: 3 Code: __HAL_I2C_DISABLE_IT(hi2c,I2C_IT_ERRI | I2C_IT_TCI| I2C_IT_STOPI| I2C_IT_NACKI | I2C_IT_ADDRI | I2C_IT_RXI | I2C_IT_RXI ); I2C...

Audio Class Microphone - STM32F4 Discovery

Posted on November 11, 2013 at 11:35Hi,I am making a SDR and implementing FM demodulation over it. We chose STM32F4 controllers for our applications yet we are successful in receiving the signal till the DAC's output.Yet I am still required to make ...

contact2 by Associate II
  • 2753 Views
  • 5 replies
  • 0 kudos

USART bootloader on STM303x

Posted on March 17, 2016 at 16:43According to section 19 of AN2606 if I want to use USART2 I have to go through pins PA2, PA3 - is this correct.Anyway, I connect to these via an FTDI USB/USART i/f chip. Bottom line is that I cannot get the STM Flash...

gbigden by Associate III
  • 3152 Views
  • 6 replies
  • 0 kudos