cancel
Showing results for 
Search instead for 
Did you mean: 

Audio Class Microphone - STM32F4 Discovery

contact2
Associate II
Posted on November 11, 2013 at 11:35

Hi,

I am making a SDR and implementing FM demodulation over it. We chose STM32F4 controllers for our applications yet we are successful in receiving the signal till the DAC's output.

Yet I am still required to make this board more fruitful to us by introducing like a USB 

Microphone

 device. It just transmits the data to the host as an audio device just like a 

microphone

 do. Please help me in making my project complete. I am using KEIL uVision for ARM.

Continuous Data -> DMA -> USB Buffer -> USB Audio Class -> Detected as USB 

Microphone

 on PC.

#usb-audio-class #stm32f4-discovery-microphone #stm32f4
This discussion is locked. Please start a new topic to ask your question.
5 REPLIES 5
Amel NASRI
ST Employee
Posted on November 12, 2013 at 09:15

Hi,

Are you facing any issue with a code you are already using? Or you need an example?

Did you checked the examples provided within the USB library (Ex: STM32_USB-Host-Device_Lib_V2.1.0\Project\USB_Device_Examples\AUDIO)?

-Mayla-

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

contact2
Associate II
Posted on November 12, 2013 at 12:22

I have seen this example, this example is for USB Speaker and I need USB Mic

Also, I am unable to run this example on STMF4Discovery.

Please help me in running this example.

skufaev
Associate II
Posted on April 28, 2014 at 20:49

Did you find working example for mic input?

spencerwang
Associate
Posted on March 18, 2016 at 09:48

Hi Mayla,

Would you please help to provide any examples about usb microphone?

Thanks a lot!

Spencer

nortowianski
Associate III
Posted on March 21, 2016 at 09:04

Type in google: 

USB �?¼�?¸�?ºÑ€�?¾Ñ„�?¾�?½ �?½�?° �?±�?°�?·�?µ STM32F4-DISCOVERY