STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to use LwIP on STM32N6570-DK board

Hi everyone,How can I use the LwIP stack to enable Ethernet on the STM32N6 board? I found a tutorial, but it was for the H5 series. Additionally, I couldn't find the LwIP middleware component in the STM32CubeN6 folder.Thanks in advance!

conflict USART and SPI

Each time I enable SPI, it works fine.However, whenever I include USART, SPI freezes, and this issue affects multiple chips I've tested.SPI and USART both work well individually.The problem seems to stem from CubeMX, which doesn't generate the code c...

MNapi by Senior III
  • 1314 Views
  • 11 replies
  • 6 kudos

Resolved! What is "hal_ppp"?

Hi, This might seem like a dumb comment, but I am reading UM1884, Description of STM32L4/L4+ HAL and low-layer drivers, and I find numerous references to "hal_ppp" or "HAL_PPP" such as the file name "stm32l4xx_hal_ppp.c" (Table 2, page 8) or "HAL_PPP...

AMacd.1 by Senior
  • 974 Views
  • 2 replies
  • 1 kudos

Resolved! STM32G431 TS_CAL2 temperature

HIAt what temperature the TS_CAL2 value for the STM32G431 is detected?In the datasheet it is reported 130 degrees while in the library "stm32g4xx_ll_adc.h" TEMPSENSOR_CAL2_TEMP is 110 degrees Thanks

STM32F429 FMC No action

Hello I want the STM32 to transmit data to the FPGA via the FMC. However, when I use the manufacturer's example and modify the return line in the FPGA, the LCD displays the modified value from the STM32 instead of the expected return line value. What...

Connoe by Associate
  • 723 Views
  • 3 replies
  • 0 kudos

Resolved! STM32 Nucleo H7S3L8 HardFault_Handler + DACCVIOL

STM32H7S3L8 – XIP app HardFault on vector fetch from XSPI (BFAR/MMFAR=0x70000004, VECTBL)MCU: STM32H7S3L8Tooling: STM32CubeIDE (HAL/CMSIS + FreeRTOS)External flash: NOR on XSPI2 (XSPIM Port 2). Bootloader sets XSPI to memory-mapped; application is li...

htxy_0-1758021070194.png
htxy by Associate III
  • 1344 Views
  • 1 replies
  • 0 kudos