HIAt what temperature the TS_CAL2 value for the STM32G431 is detected?In the datasheet it is reported 130 degrees while in the library "stm32g4xx_ll_adc.h" TEMPSENSOR_CAL2_TEMP is 110 degrees Thanks
Right, thanks,For the G431 I'm using STM32CubeIDE Version 1.7.0 with STM32Cube FW_G4 V1.4.0 because using STM32CubeIDE Version 1.8.0 with STM32Cube FW_G4 V1.5.0 and the same code the interrupts are not generated or intercepted and I don't understand ...