STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L Flash HalfPageProgram problem

Posted on April 18, 2015 at 23:00Hi,I am not able to program the flash of a STM32L151RC using ''half page'' programming.Normal programming (word by word) works fine.I have tried it using the 2 latest GCC compilers (4.8.4), and I have tried with the ...

stm32f767 and UART DMA IT (interrupts)

Posted on January 24, 2017 at 11:07Hi,How to use UART in DMA mode with interrupts IT.I use the next code to transmit, and it works perfect. HAL_DMA_Start_IT(&hdma_usart3_tx, (uint32_t)msg, (uint32_t)&huart3.Instance->TDR, strlen(msg)); huart3.Instan...

embvis by Associate III
  • 2733 Views
  • 5 replies
  • 0 kudos

USB to Ethernet bridge

Posted on January 24, 2017 at 12:53Hello,I want to make a bridge from USB to Ethernet, to give connectivity to a tablet.I am using an STM32F107RC, a DP83848CVV phyter and the CubeMX to generate the code with this configuration:I do not know how to l...

0690X000006067MQAQ.png

Mutual exclusion for HAL using FreeRTOS

Posted on January 18, 2017 at 10:51I'm going to use the different peripheral drivers (HAL) from ST with the FreeRTOS. The system will have different thread executions, and each one will use different peripherals.The question is whether the HAL imple...

0690X000006064XQAQ.png

USB Host and Composite device..

Posted on February 08, 2016 at 12:03How to make on STM32F4 USB a host with support of the Composite device?I made the project in CubeMX, but in this project there is a support of different classes of devices, but there is no support of the Composite...

mak1308 by Associate III
  • 7187 Views
  • 10 replies
  • 0 kudos