User Activity

Posted on February 10, 2017 at 09:19Hi All,I am evaluating the STM32f4 discovery board. I want to implement the USB mass storage functionality.I interfaced the SD card using the SDIO 1-bit mode.But, I want to share SD card's data in the PC use of US...
Posted on January 17, 2017 at 10:20Hello All,I am interface a SD card with STM32f4 discovery board. i am use the SPI protocol for the same.I use the IAR IDE for the development.I need the example code for further development.So, please share the exa...
Posted on January 03, 2017 at 10:16Hello All,We are interfacing the OV5642 camera module with STM32f4 discovery board.We are read the camera model no using the i2c protocol. When we are put the break point in the I2C stop condition, we can read the ...
Posted on December 24, 2016 at 06:50Hello,We are evaluating stm32f4 discovery board.we have connected the LSM9DS0 with stm32f4 via I2C communication.we are read the one default register from the LSM9DS0 accelerator,But we can not able to read this r...