STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! USBD_LL_PrepareReceive or similar after a USB Class specific SET_CURRENT request where USBD_CtlPrepareRx is used? Otherwise setup packets are no longer received.

Hi,So the way the USB class drivers are implemented is that USBD_ClassName_Setup for a SET_CURRENT request will call USBD_CtlPrepareRx to receive the SET_CURRENT data payload and then the request will be processed from the USBD_ClassName_EP0_RxReady ...

HAL_I2C_Mem_Read on SMT32L0 causes HardFault

I call this function a very large amount of times through out my entire program however in just one spot I reliably get a Hard Fault when it's called. When this line is executed, the fault occurs. (*hi2c->pBuffPtr++) = hi2c->Instance->RXDR;I called t...

bootloader without manual pin settings

helloI am using stm32l4 series microcontroller with keil mdk arm 5 programing.Had successfully completed the booting process by manually setting boot0 pin and resetting the device using flash loader demo tool. Now i wanted to do the same without manu...

prsh by Associate II
  • 2519 Views
  • 8 replies
  • 0 kudos

Resolved! "Safely" removing a USB from a system

Hi all,I am currently learning how to interface with a USB using an stm32f2 as a host.I am using the fatfs library and it is working quite well.I have a question relating how removing a USB from the system. Similar to Windows for example, they have a...

Preinstalled serial bootloader in STM32F103

Hello everybody,I'm not familiarized with hardware's industrial production. My question is about the serial (UART) built-in bootloader that comes with the Blue Pill development board. If I would like to create a new custom circuit, and print 10 test ...

Dayi by Associate
  • 1796 Views
  • 1 replies
  • 0 kudos