STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

UART hal RX interrupt modification

My scenario I have a master controller keep sending 30Bytes of data with every 500ms..Issue when use to my slave controller is :HAL_UART_Receive_IT(&huart1, varPtr, 20);the packet might not be received properly as the slave is hot swapped.. it can be...

Boot STM32H7 after power up

According to PM0253 "Programming Manual" after power up the the vector table is located at address 0x0000000. This memory is RAM memory (ITCMRAM) so how the boot can run from it if it just powered up? ​There is no memory address in it...In other CPU ...

Yood by Associate II
  • 2205 Views
  • 4 replies
  • 0 kudos

STM32F7-FFS-FreeRTOS Hard Fault

I am working with a sample project for the stm32F746G. Testing on the Discovery Board. I am using VisualGDB. The project is USB Device | MSC Host RTOS. After importing the project and tweaking a few things It did run. (However, all of these projects ...

Jona by Associate III
  • 1248 Views
  • 1 replies
  • 0 kudos

Resolved! Issue with X-NUCLEO-IDW04A1

Posted on April 13, 2018 at 01:22Hi,I recently bought the following development boards : - NUCLEO-L476RG- X-NUCLEO-IDW04A1 (Wifi expansion board)I am also using the following software packages: - STM32Cube_FW_L4_V1.11.0- STM32CubeExpansion_WIFI1_V3....

ST DFU Bootloader Issue with some USB ports

Hi community, I implemented a C# application to monitor, configure and upgrade a ST device (STM32F072). On my development notebook it works fine, but only if I connect the device via USB with the docking station or to my laptop without docking statio...

CDril by Associate
  • 2177 Views
  • 4 replies
  • 0 kudos