STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Change Timer and PWM period "on the fly" ?

Hi, I'm currently trying to set up acceleration and deceleration phases for a stepper motor. For that I'm tryin to change the frequency of the PWM [timer1] ( and the Timer [TIMER1] interrup associated). I'm working on a STM32F407-DISC. I found out t...

JTurp by Associate II
  • 2645 Views
  • 2 replies
  • 0 kudos

How can I use a Raspberry Pi to update the firmware on an STM MCU? Also, which families of STM are capable of going through such a process?

I want to update the firmware on an STM using a raspberry pi 3 that has been connected to it. How can I do so? Please help me with the names of the families of STM that are capable of going through with this process. Also, can this be done using the ...

SSoni by Associate III
  • 3064 Views
  • 3 replies
  • 0 kudos

Assertion "pbuf_free: p->ref > 0" failed at line 747 ../Middlewares/Third_Party/LwIP/src/core/pbuf.c Received too many bytes! Droping client.

Hello Everyone,I am using STM32F429ZIT MCU and Modbus TCP library provided by FreeModbus.After attaching TCP library to my application code, i am getting below errors.In modbus TCP library , inside portTCP.c , if i am commenting prvvMBPortReleaseClie...

0690X00000896dsQAA.png 0690X00000896egQAA.png

Anything new in USB of F7 and other newer STM32s ?

Can anybody comment what is new in USB controllers of STM32F7 and new STM32L... compared to F2 or F4? Besides of built-in HS PHY. Do they have same IP core(s)? Anything improved in software? Will USB host library support hub functionality?We're gener...

Pavel A. by Super User
  • 657 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.