STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32U5 with DMA request AND trigger.

I have GPDMA working on STM32U5 with a circular buffer.  However, when I add a GPDMA "trigger" to the setup, the DMA no longer works. GPDMA1_C2TR2.TRIGPOL=2 GPDMA1_C2TR2.TRIGSEL=11 GPDMA1_C2TR2.TRIGM=3 LPTIM1 setup to clock away at a 50% duty cycle. ...

STM32H7S3V8T6 timer triggered DMA

Hi All, Trying to setup timer triggered DMA for the STM32H7S3V8T6 micro and cannot seem to get it workingI have tried a number of things and eventually resorted to asking chatGPT but so far no dice... What I want to achieve1. Timer 1 toggles CH1 outp...

JShro by Associate III
  • 710 Views
  • 1 replies
  • 0 kudos

DALI 2 DT8 Tuneable White software stack

Does anyone know if there are any software stacks available through ST that support DALI 2 colour tuneable (DT8) control gear devices (LED drivers). I can see that ST have a third party offering from MBS Solutions that claims to offer full DALI2 supp...

Bill2 by Associate II
  • 1931 Views
  • 7 replies
  • 2 kudos

OSC with STM32G4

Hello,I have an STM32G431 here that sends messages to a PC via MIDI. These are translated into OSC messages by a bridge and then interpreted by lighting control software. I would like to eliminate the intermediate step via the bridge and transmit the...

Resolved! STM32 CAN Bus skips some messages

Hi, I am using three STM32 devices for CAN communication:HardwareDevice A: STM32G431 (FDCAN)Device B: STM32F303 (Classic CAN)Device C: STM32H7A3 (FDCAN)SetupA sends a continuous sequence of commands to B.B processes each command and replies to A over...

Whats the problem with USB Host HID

Hello.I have problem using STM32 USB Host HID. I`m stuck in the USBH_Process() function in usbh_core.c, or its better to say stuck in USBH_HID_Process() function in usbh_hid.c file. I am trying to connect a USB keyboard to my own designed stm32f407zg...

0693W00000BZsMjQAL.png 0693W00000BZsMGQA1.png 0693W00000BZsNhQAL.png 0693W00000BZsSYQA1.png
HSh..1 by Associate II
  • 4250 Views
  • 6 replies
  • 1 kudos