STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to switch between MSD and FatFs?

Hi I like to use my small mcu system (stm32f401 with 4bit SDIO and USB-Device) in the follow way:If USB is plugged in -> the system should behave like a msd on a windows machine.If USB is not plugged in -> the system should read the files from the sd...

CFosc by Associate
  • 796 Views
  • 0 replies
  • 0 kudos

STM32F413VGT uart9 baud rate problem

There is a bug to set baud-rate of uart9.If I set it to 9600, it works as 19200.I think it is a problem of driver code.The UART9 and UART10 should use PCLK2 but the code uses PLCK1.Please check below.My environment:Win 10. 1809STM32CubxMX version 5.2...

TKim.11 by Associate
  • 888 Views
  • 0 replies
  • 0 kudos

Is there any good Can periephal examples available?

The title pretty much says it all, to me it seems to be impossible to get the CAN periephal running with the HAL codes.loopback works all night, next it crashes to first message.i can sniff my car's canbus, then i cant.is there any alternative availa...

JoniS by Senior
  • 706 Views
  • 0 replies
  • 0 kudos

CCA02M1 microphone example project code size

We've bought NucleoF401 and CCA02M1 boards. But example project provided by ST about 39KB, this is much more than free limit of Keil5. How can we use examples with free Keil version? These are development boards for everyone(students,hobbiests..), wh...

BISIK.18 by Associate II
  • 750 Views
  • 0 replies
  • 0 kudos

STM32F1xx_HAL_PCD -- wrong EP_IN/EP_OUT

HAL v1.7.0, stm32f1xx_hal_pcd.c, line 199During OUT EP init we have IN EPShould I fix it on my own? for (index = 0U; index < 15U ; index++) {  hpcd->OUT_ep[index].is_in = 0U;  hpcd->OUT_ep[index].num = index;  hpcd->IN_ep[index].tx_fifo_num = index; ...

RBaly by Associate
  • 595 Views
  • 0 replies
  • 0 kudos

PLL3 as I2C123 peripheral source clock on STM32H7

If the PLL3 is selected as I2C peripheral source clock, the Bits RCC_D2CCIP2R_I2C123SEL are not initialized correctly.In function HAL_RCCEx_PeriphCLKConfig() the PLL3 R Divider gets updated but the clock selection is not set to "1". In my opinion, th...

MGall.9 by Associate
  • 1040 Views
  • 0 replies
  • 1 kudos

STM32 System Memory DFU Bootloader Temperature Issues

Hi,we intend to use the STM32F479 in an industrial application where ambient temperatures might vary, and we would like to use the system memory dfu as a backup bootloader. In AN2606 I found the following note:„For STM32 devices embedding bootloader ...

IHC by Associate
  • 1210 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.