STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Multiple USB descriptor ( RNDIS + VCP)

Chip set : STM32F413xxI would like to implement RNDIS driver + VCP(FS).I wonder that usb descriptor is available or not for this combination.Descriptor was modified for this.VCP was enumerated but RNDIS was not enumerated. error code is 10 from windo...

YChun.5 by Associate
  • 795 Views
  • 0 replies
  • 0 kudos

Resolved! STM32L4xx HAL Library USB bug. Function USB_WritePMA does not work properly when compiled with "-O3" option.

I used latest CubeMX version and found another one bug in stm32l4xx_ll_usb.c generated by it. If you will compile code using "-O3" optimization level, function USB_WritePMA will not work properly. /** * @brief Copy a buffer from user memory area to ...

Leave DFU mode without unplugging cable

Hi,We are looking for a way to leave DFU mode (and the bootloader) and jump to the application without having to follow the mechanism of issuing the "Leave DFU" command, and unplugging the USB cable within the allotted 10 seconds.Is there another way...

STM32F103C8T6 ST-Link Bootloader Flashing

Hello!I'm new here, so please and sorry for the request but thoroughly explain your answers thankyou.I have an STM32F103C8T6 Board and a ST-Link V2. I can send sketches from the arduino IDE just fine using ST-Link, but neither UART(Serial) nor USB(ST...

KAyou by Associate II
  • 5466 Views
  • 3 replies
  • 0 kudos

how on stm32f765zi read flags? i2c specific format

Hello.Sorry for my bad English:) I am trying to read flag on the device MLX90614. datasaheet Page 23. The format of a SMBus transaction which reads flags is: i.e i must send start->slave address->command and right away without send repeat start recei...

0690X000008isnLQAQ.jpg 0690X000008it2zQAA.jpg
User.5 by Associate
  • 888 Views
  • 0 replies
  • 0 kudos

HAL_SAI_FlushRxFifo function implementation

On the UM1725, DocID025834 Rev 5, par 57.2.1, pag. 766 A function called HAL_SAI_FlushRxFifo() is contemplated among the "SAI HAL driver additional function list".On the hal driver, this function is declared on the comments but it is not implemented....

raffin by Associate III
  • 748 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.