HAL_SAI_FlushRxFifo function implementation
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2019-06-18 5:24 AM
On the UM1725, DocID025834 Rev 5, par 57.2.1, pag. 766 A function called HAL_SAI_FlushRxFifo() is contemplated among the "SAI HAL driver additional function list".
On the hal driver, this function is declared on the comments but it is not implemented.
Is there an implementation available?
I have a huge delay on the Rx which disappears, while debugging, if I put a breakpoint on the audio task and then restart it.
Thank you in advance.
Labels:
- Labels:
-
SAI
-
STM32Cube MCU Packages
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0