STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Clock tree frequency values duplication in code

Hello,It seems that most examples (stm32cubeh7) are independent in clock tree values, which is exactly the correct way to do it, yet some of the examples are using hardcoded values duplicated from clock tree (duplication) which seems like a bad idea ...

ranran by Senior II
  • 501 Views
  • 0 replies
  • 0 kudos

identifier"I2C handler TypeDef" is undefined.

I am merging two projects .One project is wrote in stm32f401RE and another one is stm32f429i-discovery board.I have already included all path and build the project.It shows error like identifier is undefined.only one file path is not included.But i g...

NS.16 by Associate II
  • 1220 Views
  • 1 replies
  • 0 kudos

Resolved! CRITICAL: stm32h7xx_hal_tim_ex.h wrong defines

Dear STM, please fix the defines in stm32h7xx_hal_tim_ex.h as at least TIM_TIMx_ETR are either empty or wrong, according to the datasheet. Here is a short example, _NOT_ stating all incorrect positions:NOW, IN THE FILE stm32h7xx_hal_tim_ex.h in STM32...

Max Rest by Associate II
  • 867 Views
  • 2 replies
  • 1 kudos

EEPROM EMULATION STM32f103

How can I store characters in flash memory of STM32F103 using HAL C coding?? I am able to store hex values in flash but no idea on how to save char values.

sne_123 by Associate III
  • 690 Views
  • 1 replies
  • 0 kudos

STM32F4 USB CDC and MSC class to be used for both Device-to-Host communication and Device microSD reading ? Or only CDC ?

This question is related to the code design in such a scenario when host and device communicate over USB for two purposes: two-way communication (CDC) and also host is reading the content of the Device' microSD card. The CDC mode is required in this ...

eBirdman by Senior II
  • 1183 Views
  • 2 replies
  • 0 kudos