2019-03-08 4:35 AM
Dear STM,
please fix the defines in stm32h7xx_hal_tim_ex.h as at least TIM_TIMx_ETR are either empty or wrong, according to the datasheet. Here is a short example, _NOT_ stating all incorrect positions:
NOW, IN THE FILE stm32h7xx_hal_tim_ex.h in STM32Cube_FW_H7_V1.3.2 :
#define TIM_TIM5_ETR_GPIO (0x00000000) /* !< TIM5_ETR is connected to GPIO */
#define TIM_TIM5_ETR_SAI2_FSA (0x00000000) /* !< TIM5_ETR is connected to SAI2 FS_A */
#define TIM_TIM5_ETR_SAI2_FSB (0x00000000) /* !< TIM5_ETR is connected to SAI2 FS_B */CORRECT, according to RM0433 Rev 5, p. 1686/3247
#define TIM_TIM5_ETR_GPIO (0x00000000) /* !< TIM5_ETR is connected to GPIO */
#define TIM_TIM5_ETR_SAI2_FSA (0x00001000) /* !< TIM5_ETR is connected to SAI2 FS_A */
#define TIM_TIM5_ETR_SAI2_FSB (0x00002000) /* !< TIM5_ETR is connected to SAI2 FS_B */This is a critical bug.
Thanks,
Maximilian Rest
Solved! Go to Solution.
2019-03-08 5:45 AM
Hello Max,
thank you for reporting,
This bug is already fixed internally. It should be in a next release.
2019-03-08 5:45 AM
Hello Max,
thank you for reporting,
This bug is already fixed internally. It should be in a next release.
2019-03-08 5:51 AM
Hi Mike,
thanks for your quick reply, sounds good. I hope you meant in _the_ next release though, because fixing it manually and overwriting it each time cube regenerates the files is quite ... annoying.
Best,
Max