STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

HAL User Manual and CAN in 1.8.0

I'm trying to develop application using CAN driver. It looks like the STM32F1 HAL User Manual (UM1850) is outdated.The processor is STM32F103RGT6Where can I find documentation of CAN driver for 1.8.0 Cube version? Or maybe there is somewhere the upda...

Maciej by Associate II
  • 1274 Views
  • 1 replies
  • 0 kudos

CubeMX deleted my usbpd_dpm_user.c

Hello there,I don't know if I can call this a bug, but it shouldn't happen at all.Thing goes like this: I have a STM32G071, I enabled UCPD1 and 2, also CMSIS, USBPD library in CubeMXI generated code for SW4STM32, I write my custom board code in usbpd...

JChau by Associate II
  • 1366 Views
  • 2 replies
  • 0 kudos

CubeMX/HAL RCC_MCO3 bug

When generating code for the STM32L051C8Tx and STM32L053C8Tx MCUs using CubeMX I am experiencing a build error when setting channel 1 of TIM21 in input capture mode. The following line is added in main.c within the void SystemClock_Config(void) funct...

SPetr.6 by Associate III
  • 968 Views
  • 1 replies
  • 0 kudos