Skip to main content
Sergey Starovoitov
Associate
June 5, 2018
Question

Bug report: CubeMX CMSIS generation error

  • June 5, 2018
  • 1 reply
  • 805 views
Posted on June 05, 2018 at 11:18

Hello, everybody! I tried to generate initialization code for my STM32F103CB-based project with STM32CubeMX 4.25.1 and 1.6.1 version of firmware, and CubeMX generated Drivers/CMSIS/... folders, but they were empty, and TrueStudio got error:

In file included from ../Drivers/STM32F1xx_HAL_Driver/Inc/stm32f1xx_hal_rcc.h:45:0,

                 from ../Inc/stm32f1xx_hal_conf.h:219,

                 from ../Drivers/STM32F1xx_HAL_Driver/Inc/stm32f1xx_hal.h:46,

                 from ../Inc/rtc.h:47,

                 from ..\Src\rtc.c:41:

../Drivers/STM32F1xx_HAL_Driver/Inc/stm32f1xx_hal_def.h:46:23: fatal error: stm32f1xx.h: No such file or directory

 &sharpinclude 'stm32f1xx.h'

So, i filled these folders by the CMSIS files, generated by the older version of CubeMX, and they are OK, but Drivers\CMSIS\Device\ST\STM32F1xx\Include folder cleans every time, I regenerate code by CubeMX. Please fix this issue, or show me, where Iwas wrong.

Thank you!

#stm32cube---bug-report #cmsis
This topic has been closed for replies.

1 reply

Nawres GHARBI
ST Technical Moderator
June 8, 2018
Posted on June 08, 2018 at 13:20

Hi Sergey, 

I tested with your ioc and all is generated correctly. 

May be it a corrupted file in your env, please do a save as and change the project folder and try to generate from scratch

if it is ok just overwrite with your changes on the new project